AXIS#.VL.FBSOURCE

Description

This parameter determines the feedback source to be used by the velocity loop.

Value Definition
0 Defers selection to AXIS#.IL.FBSOURCE - this is the default, and uses the value which is being used for commutation
1 Selects FB1 (connector X1)
2 Selects FB2 (connector X2)
3 Selects FB3 (connector X23)
4 Selects FB4 (connector X21)
5 Selects FB5 (connector X22)

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 5

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.FBSOURCE

5011h

24h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6026

1

6026 (0x178a)

AXIS1.VL.FBSOURCE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.VL.FBSOURCE

6026

Unsigned8

Read/Write

-

Related Topics

Velocity Loop